Torque limiting three-lobed knobs GN 3664 are used when the manually applied torque is to be set or limited.
When turned clockwise, the torque mechanism of the three-lobed knob triggers an “over-engagement” as soon as the specified torque is reached. When turned counter-clockwise, the mechanism locks up to disable any torque limiting. This ensures that a maximum permissible torque is not exceeded, e.g. when tightening, while the torque required for loosening is always transmitted reliably.
Specification
Knob body
Technopolymer (Polyamide PA-HP)
Glass fiber reinforced
Black, matte finish
Torque mechanism
Steel, hardened
Other components
Steel, blackened finish
Cover
Plastic, light gray
RoHS
On request
Other dimensions of threaded studs as per GN 300
Other inserts with special-tipped threaded studs as per GN 306
Other torques
Torque limiting turning counter-clockwise, or turning counter-clockwise and clockwise
This article is RoHS-compliant in application of Annex III., which means it complies with EU Directive 2011/65/EU, including extension (2015/863/EU), for restricting the use of certain hazardous substances in electrical and electronic devices. The Directive regulates the use of hazardous substances in devices and components. The implementation in national law is summarily described with RoHS(Restriction of (the use of certain) hazardous substances)).
Weight: 0.164 lbs
If weight is not listed, please contact our Sales Department for additional information regarding weight. Phone: 800-877-8351
Beginning June 15, 2024, we will implement a price adjustment. Some items will have a price decrease, while others will increase. The adjustment helps ensure our commitment to providing our customers with the best products and services.
We will honor current published prices through June 14, 2024.
Customers with pricing agreements will not be effected until annual pricing is reviewed.
Thank you J.W. Winco
An error has occurred!
We have received your callback request and will contact you soon.