Guide rollers GN 753.1 can be used as guides, bearings or supports for small to medium loads. They can also be used to create custom linear guide rail systems.
The radial load capacity rating given in the table should be understood as a guide value at which the guide rollers achieve a lifetime performance of at least 656,167 ft (200,000 m). The conditions for achieving this lifetime performance are a speed of 1.3 ft/s (0.4 m/s), a clean, dry, level, smooth and hard surface to roll against and an operating temperature between 59 °F and 86 °F (15 °C and 30 °C). In general, the guide rollers should not be used under axial load.
Specification
Outer race
Plastic (Polyacetal POM)
Operating temperature:
-4 °F to 212 °F (-20 °C to 100 °C)
This article is RoHS-compliant in application of Annex III., which means it complies with EU Directive 2011/65/EU, including extension (2015/863/EU), for restricting the use of certain hazardous substances in electrical and electronic devices. The Directive regulates the use of hazardous substances in devices and components. The implementation in national law is summarily described with RoHS(Restriction of (the use of certain) hazardous substances)).
Weight: 0.013 lbs
If weight is not listed, please contact our Sales Department for additional information regarding weight. Phone: 800-877-8351
Beginning June 15, 2024, we will implement a price adjustment. Some items will have a price decrease, while others will increase. The adjustment helps ensure our commitment to providing our customers with the best products and services.
We will honor current published prices through June 14, 2024.
Customers with pricing agreements will not be effected until annual pricing is reviewed.
Thank you J.W. Winco
An error has occurred!
We have received your callback request and will contact you soon.