With clamping arm extenders GN 809.1, various toggle clamps with a “solid clamping arm” can be easily and quickly extended. The slot of the extender corresponds to the dimensions of the respective toggle clamp size with “U-bar clamping arm” and is therefore compatible with all accessories, such as flanged washers, spindle assemblies, etc.
For assembly, the clamping arm extenders are placed onto the clamping arms of the toggle clamps and bolted into place. The required holes in the clamping arm of the toggle clamp must be made by the user.
All parts are supplied in a non-assembled set. Two flanged washers are included for fastening the spindle assembly.
This article is RoHS-compliant in application of Annex III., which means it complies with EU Directive 2011/65/EU, including extension (2015/863/EU), for restricting the use of certain hazardous substances in electrical and electronic devices. The Directive regulates the use of hazardous substances in devices and components. The implementation in national law is summarily described with RoHS(Restriction of (the use of certain) hazardous substances)).
Weight: 0.218 lbs
If weight is not listed, please contact our Sales Department for additional information regarding weight. Phone: 800-877-8351
Beginning June 15, 2024, we will implement a price adjustment. Some items will have a price decrease, while others will increase. The adjustment helps ensure our commitment to providing our customers with the best products and services.
We will honor current published prices through June 14, 2024.
Customers with pricing agreements will not be effected until annual pricing is reviewed.
Thank you JW Winco
An error has occurred!
We have received your callback request and will contact you soon.