WN 306 adjustable levers are the result of modern industrial design: glass fiber reinforced thermoplastic with molded-in stainless steel inlay.
They have proven to be ideal wherever parts have to be clamped in a confined space or in a particular lever position. The insert is connected to the lever via serrations that can easily be disengaged.
Pulling the lever upwards disengages the serrations, allowing it to be swiveled to the ideal clamping position. When releasing the lever, the serrations automatically re-engage.
The brass and plastic tipped studs (types MS / KU) help to avoid damage to the workpiece being clamped.
The hardened tipped stud (type DZ) provides an oval point-shaped pressure point.
The swivel thrust pad (type KD) is easily clipped on and taken off. Thrust pads are supplied unmounted.
Specification
Lever body PlasticKT
Nylon thermoplastic
Temperature resistant up to 230 °F (110 °C)
This article is RoHS-compliant in application of Annex III., which means it complies with EU Directive 2011/65/EU, including extension (2015/863/EU), for restricting the use of certain hazardous substances in electrical and electronic devices. The Directive regulates the use of hazardous substances in devices and components. The implementation in national law is summarily described with RoHS(Restriction of (the use of certain) hazardous substances)).
Weight: 0.055 lbs
If weight is not listed, please contact our Sales Department for additional information regarding weight. Phone: 800-877-8351
Beginning June 15, 2024, we will implement a price adjustment. Some items will have a price decrease, while others will increase. The adjustment helps ensure our commitment to providing our customers with the best products and services.
We will honor current published prices through June 14, 2024.
Customers with pricing agreements will not be effected until annual pricing is reviewed.
Thank you JW Winco
An error has occurred!
We have received your callback request and will contact you soon.